How to load a compiled C application on 8mPLUS EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to load a compiled C application on 8mPLUS EVK

1,343 Views
ShivM
Contributor II

Hi,

I have compiled a C Application for IMX 8M PLUS EVK.

Now I want to load the C application on IMX 8M PLUS EVK.. Not the entire boot image..

I searched UUU it has instructions to load the boot image but not just a regular application image

0 Kudos
Reply
3 Replies

1,339 Views
Yuri
NXP Employee
NXP Employee

@ShivM 
Hello,

   You may try to use WinSCP.

Regards,
Yuri.

0 Kudos
Reply

1,333 Views
ShivM
Contributor II

Hi Yuri,

 

I tried using.. Is there any documentation what should be the IP address of Host?

I used to load other(no nxp) boards using WinSCP and would like to do that. I will need the IP addresses of Host PC.

0 Kudos
Reply

1,327 Views
Yuri
NXP Employee
NXP Employee

 You need IP address of the target board. Its IP can be received, using DNS or configured 
manually.

 

~Yuri.

0 Kudos
Reply