How to limit the i.mx6q core speed/core number to reduce power consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to limit the i.mx6q core speed/core number to reduce power consumption

1,499件の閲覧回数
lonsn
Contributor I

Hi,

We designed a custom i.mx6q board based on sabresd. The CPU is very hot when playing video. Since the i.mx6q performance is high enough for us now and we only care the high temp stability.  We want to find some way to decrease the cpu power consumption more. The system is Android 5.0 and 3.10 kernel. We already disabled the unused module in dtb file. 

How can I limit the i.mx6q cpu frequency(< 792MHz) ?

Can I decrease the used core numbers to 2 without replacing the chip to dual version?

How can I decrease the GPU performance to decrease the power since we only care video play and have not much requirement for the GPU.

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

1,337件の閲覧回数
andrzejdziedzic
Contributor IV

Hi

Based on my tests:

- cores can be disabled as described by Yuri - but it won't reduce the temperature

- reducing CPU frequency to minimum also won't help too much.

0 件の賞賛
返信

1,337件の閲覧回数
lonsn
Contributor I

Yes, I have tested the cpu core number decrease, totally no any difference in power consumption.

0 件の賞賛
返信

1,337件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments below.

1.

  Please use section 4 (Reducing Power Consumption) of the following

app note.

“i.MX 6Dual/6Quad Power Consumption Measurement”

http://cache.nxp.com/files/32bit/doc/app_note/AN4509.pdf

2.

  Kernel boot parameter “maxcpus” may be used to define maximum

number of processors. Please refer to section 4 (Kernel Boot Parameters)

of “i.MX_Linux_Release_Notes.pdf”

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信