How to limit USB 2.0 channels to Full-speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to limit USB 2.0 channels to Full-speed

1,807件の閲覧回数
admin
Specialist II

Saved FAQ from Freescale.com for information only:

Topic: USB

 

Question.  How to limit USB 2.0 channels to Full-speed (12Mbit)?

 

Answer.  Software should set the PFSC bit (bit 24) in the PORTSC register during USB controller init and prior to setting the RS bit in the USBCMD register (start controller). The port will than work in full speed only. However, the ULPI interface speed will remain 60 MHz so the CLK will still be at 60 MHz.

 

To avoid issues one may try to use non-high speed (if present) PC USB port.  Also please check (USB) device descriptors, what options are supported. Particularly, pay attention on bcdUSB field (USB spec Release Number - if set for 1.1 the host will not try high speed).

 

 Related Products:

 i.MX Applications Processors > i.MX51 Processors > i.MX512, i.MX513, i.MX514, i.MX515, i.MX516

タグ(1)
0 件の賞賛
返信
0 返答(返信)