How to keep i.MX6Q VDDUSB_CAP in 3v at suspend mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to keep i.MX6Q VDDUSB_CAP in 3v at suspend mode?

599 Views
m_c
Senior Contributor I

Run mode, USB_VBUS supply 5V, VDDUSB_CAP=3V

suspend mode, USB_VBUS supply 5V, VDDUSB_CAP=2V

How to keep i.MX6Q VDDUSB_CAP in 3v at suspend mode?

pastedImage_2.png

pastedImage_1.png

Labels (1)
0 Kudos
1 Reply

364 Views
art
NXP Employee
NXP Employee

In the suspend mode, the USB core is powered off, so, there is no way (and no need) to keep the VDD_USB_CAP voltage at fixed level.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos