How to keep enabled splash screen on LCD while booting from u-boot to kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to keep enabled splash screen on LCD while booting from u-boot to kernel

5,510件の閲覧回数
Deepu
Contributor III

Hi Freescale Team ,

While booting when the control goes to kernel from u-boot ,the  splash screen intialised by u-boot will get turned off and will come again only after kernel is booted. When I cross checked the u-boot I saw ipuv3_fb_shutdown function to be called from arch_preboot_os which is called from do_bootm function.

In u-boot mailing lists ,it is shown that they added this fix to disable video as the kernel was hanging with video enabled.

 

http://patchwork.ozlabs.org/patch/185914/

So can u suggest any method to keep LCD enabled through out the booting process that is from u-boot to kernel?

Message was edited by: Deepu James

ラベル(7)
1 返信

2,875件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

In Android QuickStart guide it mentiones you should pass "fb0base=0x27b00000" to kernel at bootime when using LVDS screen. This may need adjusting depending on your u-boot setup (how/where memory is allocated for framebuffer).