How to interface VGA display with imx6 Sabre Ai

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to interface VGA display with imx6 Sabre Ai

2,301 次查看
ramakrishnanven
Contributor II

Development Environment

Host - Windows 7, 64 bit

Board - imx6 Sabre AI

BSP - QNX SDP 6.6

Booting Type - SD Card

Things done so far

     1. I have downloaded QNX Neutrinos SDP 6.6 and installed in Windows 7, 64 Bit

     2. Using QNX Momentics to compile and got ifs-mx6x-sabreARD.raw file

     3. Formatted the SD card, Partioned the SD Card, Placed U-Boot and .raw file in the SD Card

     4. Used "HyperTerminal" in Windows host and connected to imx6 Board

     5. imx6 is booting with Qnx Neutrino and is displayed in the HyperTerminal

Things needed to do

     1. I have to interface a display with imx6 and should get an output on the display
     2. I am using HDMI for taking the video output

     3. I have connected HDMI to VGA converter and connected a VGA Monitor.  

Issue:

     I could not get any display in the VGA Monitor. What should I do to get a display in the VGA Monitor

Thanks in Advance..

Message was edited by: Ramakrishnan Venkatraman

标签 (1)
标记 (3)
2 回复数

1,594 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

1,594 次查看
ramakrishnanven
Contributor II

Thanks for your information. It was my first post. I edited spaces to imx Community

0 项奖励
回复