Hi Team,
I am using imx6ul custom board and interface to Display-tech lcd (1024x600).
Some changes in device tree file but lcd not working. First trying to configure display next touch.
We are given GPIO pin for back-light control and able to changing.
My device tree :
&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif_dat
&pinctrl_lcdif_ctrl>;
display = <&display0>;
status = "okay";
display0: display {
bits-per-pixel = <16>;
bus-width = <24>;
display-timings {
native-mode = <&timing0>;
timing0: timing0 {
clock-frequency =<50000000>;
hactive = <1024>;
vactive = <600>;
hfront-porch = <0>;
hback-porch = <0>;
hsync-len = <176>;
vback-porch = <0>;
vfront-porch = <0>;
vsync-len = <25>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <0>;
};
};
};
};
pinctrl_lcdif_dat: lcdifdatgrp {
fsl,pins = <
MX6UL_PAD_LCD_DATA00__LCDIF_DATA00 0x79
MX6UL_PAD_LCD_DATA01__LCDIF_DATA01 0x79
MX6UL_PAD_LCD_DATA02__LCDIF_DATA02 0x79
MX6UL_PAD_LCD_DATA03__LCDIF_DATA03 0x79
MX6UL_PAD_LCD_DATA04__LCDIF_DATA04 0x79
MX6UL_PAD_LCD_DATA05__LCDIF_DATA05 0x79
MX6UL_PAD_LCD_DATA06__LCDIF_DATA06 0x79
MX6UL_PAD_LCD_DATA07__LCDIF_DATA07 0x79
MX6UL_PAD_LCD_DATA08__LCDIF_DATA08 0x79
MX6UL_PAD_LCD_DATA09__LCDIF_DATA09 0x79
MX6UL_PAD_LCD_DATA10__LCDIF_DATA10 0x79
MX6UL_PAD_LCD_DATA11__LCDIF_DATA11 0x79
MX6UL_PAD_LCD_DATA12__LCDIF_DATA12 0x79
MX6UL_PAD_LCD_DATA13__LCDIF_DATA13 0x79
MX6UL_PAD_LCD_DATA14__LCDIF_DATA14 0x79
MX6UL_PAD_LCD_DATA15__LCDIF_DATA15 0x79
MX6UL_PAD_LCD_DATA16__LCDIF_DATA16 0x79
MX6UL_PAD_LCD_DATA17__LCDIF_DATA17 0x79
MX6UL_PAD_LCD_DATA18__LCDIF_DATA18 0x79
MX6UL_PAD_LCD_DATA19__LCDIF_DATA19 0x79
MX6UL_PAD_LCD_DATA20__LCDIF_DATA20 0x79
MX6UL_PAD_LCD_DATA21__LCDIF_DATA21 0x79
MX6UL_PAD_LCD_DATA22__LCDIF_DATA22 0x79
MX6UL_PAD_LCD_DATA23__LCDIF_DATA23 0x79
>;
};
Boot Logs :
imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/flexcan1grp
imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/pwm1grp
backlight supply power not found, using dummy regulator
21c8000.lcdif supply lcd not found, using dummy regulator
mxsfb 21c8000.lcdif: failed to find mxc display driver
Console: switching to colour frame buffer device 128x37
mxsfb 21c8000.lcdif: mxs wait for pan flip timeout
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: loaded firmware 3.3
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 69, base_baud = 5000000) is a IMX
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 70, base_baud = 5000000) is a IMX
imx-rng 2284000.rngb: iMX RNG Registered.
[drm] Initialized
[drm] Initialized vivante 1.0.0 20120216 on minor 0
edt_ft5x06 1-0038: touchscreen probe failed
input: iMX6UL Touchscreen Controller as /devices/soc0/soc/2000000.aips-bus/2040000.tsc/input/input2
Dear igor,
Thanks for reply,
Device tree file changes as per the above link, while booting observed one issues.
Logs :
imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/flexcan1grp
imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/pwm1grp.
How to calculate the address value ( MX6UL_PAD_LCD_DATA00__LCDIF_DATA00 0x79) -> 0x79.
Hi naveen
>How to calculate the address value ( MX6UL_PAD_LCD_DATA00__LCDIF_DATA00 0x79) -> 0x79.
one can look at sect.30.5.229 SW_PAD_CTL_PAD_LCD_DATA00 SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_LCD_DATA00) i.MX6UL Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf
Best regards
igor
Thanks for the reply,
issue :1 . Interfaced LCD is 24bit and developed board is 18 bit, for 24bit lcd 6 more pins are required.
PWM and CAN pins are added for 24 but lcd. I commented in my device tree file but some errors are observed.
My device tree configuration :
compatible = "pwm-backlight";
pwms = <&pwm1 0 20000>;
brightness-levels = <0 4 8 16 32 64 128 255>;
default-brightness-level = <6>;
status = "disable";
};
&pwm1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm1>;
status = "disabled";
}; pinctrl_pwm1: pwm1grp {
fsl,pins = <
/*MX6UL_PAD_LCD_DATA00__PWM1_OUT 0x110b0*/
>;
};
Error logs :
imx6ul-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ul-evk/pwm1grp
2. lcif driver loading errors are observed in logs.
3. some pan flip timout error observed.
1. I am able to load the driver and created interrupts.
root@imx6ul-var-dart:~# cat /proc/interrupts
220: 0 gpio-mxc 17 Edge edt-ft5x06
2. Input device created
[ 2.426747] input: EP0790M09 as /devices/soc0/soc/2100000.aips-bus/21a4000.i2c/i2c-1/1-0038/input/input1
3. When press touch not responding
root@imx6ul-var-dart:~# evtest /dev/input/touchscreen0
Input driver version is 1.0.1
Input device ID: bus 0x18 vendor 0x0 product 0x0 version 0x0
Input device name: "EP0790M09"
Supported events:
Event type 0 (EV_SYN)
Event type 1 (EV_KEY)
Event code 330 (BTN_TOUCH)
Event type 3 (EV_ABS)
Event code 0 (ABS_X)
Value 0
Min 0
Max 1023
Event code 1 (ABS_Y)
Value 0
Min 0
Max 599
Event code 47 (ABS_MT_SLOT)
Value 0
Min 0
Max 4
Event code 53 (ABS_MT_POSITION_X)
Value 0
Min 0
Max 1023
Event code 54 (ABS_MT_POSITION_Y)
Value 0
Min 0
Max 599
Event code 57 (ABS_MT_TRACKING_ID)
Value 0
Min 0
Max 65535
Properties:
Property type 1 (INPUT_PROP_DIRECT)
Testing ... (interrupt to exit)
4. I able to read device id and some other commands data using below command
root@imx6ul-var-dart:~# i2cget -y -f 1 0x38 0x02 (Number of touch points)
0x03
root@imx6ul-var-dart:~# i2cget -y -f 1 0x38 0x00 (working mode)
0x00
How to calibrate touch screens and run my qt qtplication.
DART-6UL was developed and supported by Variscite, one can post question on its wiki:
DART-6UL Yocto Morty Build Yocto release - Variscite Wiki
Best regards
igor
Dear Igor,
Thanks for the reply, This issues already posted but no reply ..Please give me any solution for this issues.
Regards,
Nv
Hi naveen
one can try with latest nxp bsps from source.codeaurora.org/external/imx/linux-imx
imx6ul-14x14-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
use appropriate kernel boot parameter which can be found in linux documentation (Release Notes) on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------