How to interface 18-bit lcd with i.MX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to interface 18-bit lcd with i.MX6ULL

4,063件の閲覧回数
Gallopwc
Contributor I

I am trying to interface 18-bit lcd with i.MX6ULL. According to the user manual, data pins used in 18-bit DOTCLK mode is LCD_DATA00 - LCD_DATA17, so I connect the display like this:

LCD_DATA00 ------ B0

LCD_DATA01 ------ B1

LCD_DATA02 ------ B2

LCD_DATA03 ------ B3

LCD_DATA04 ------ B4

LCD_DATA05 ------ B5

LCD_DATA06 ------ G0

LCD_DATA07 ------ G1

LCD_DATA08 ------ G2

LCD_DATA09 ------ G3

LCD_DATA10 ------ G4

LCD_DATA11 ------ G5

LCD_DATA12 ------ R0

LCD_DATA13 ------ R1

LCD_DATA14 ------ R2

LCD_DATA15 ------ R3

LCD_DATA16 ------ R4

LCD_DATA17 ------ R5

 

The kernel version used is 4.1.15, and my DTS is as follow

&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif_dat
&pinctrl_lcdif_ctrl>;
display = <&display0>;
status = "okay";

display0: display {
bits-per-pixel = <32>;
bus-width = <18>;

display-timings {
native-mode = <&timing0>;
timing0: timing0 {
clock-frequency = <6300000>;
hactive = <320>;
vactive = <240>;
hfront-porch = <65>;
hback-porch = <10>;
hsync-len = <5>;
vback-porch = <7>;
vfront-porch = <12>;
vsync-len = <3>;

de-active = <1>;
hsync-active = <0>;
vsync-active = <0>;
pixelclk-active = <0>;
};
};
};
};

But pictures are not display in right color, there seems to be a lack of green, I have shown a QT routine (animatedtiles) on the screen, it is supposed to be dark green, but now it's dark red. The boot information on the screen should be white, but now it's blue. Images are clear except for the color. I don't know if the connection to the display is not right, or there is something wrong with my dts configuration.

0 件の賞賛
返信
4 返答(返信)

4,020件の閲覧回数
Gallopwc
Contributor I

Thanks for your reply, @Sanket_Parekh .

Sure, I have attached the datasheet and the picture showed on my display.  As you can see, original qt example is dark green, but it's dark red on my display.

Thanks & Regards

Gallopwc

0 件の賞賛
返信

3,989件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

the R pins should be connected to the most significant bits, then G and finally B.

So for this 18-bit RGB LCD:

R[5:0] <-> LCD_D[21:16]

G[5:0] <-> LCD_D[13:08]

B[5:0] <-> LCD_D[05:00]

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信

4,029件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

I hope you are doing well.

Can you please share the datasheet of the display to debug this issue further?

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信

4,026件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

Waiting for your answer.

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信