How to interconnect i.MX8MM with FPGA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to interconnect i.MX8MM with FPGA

ソリューションへジャンプ
3,706件の閲覧回数
chao
Contributor II

Hello, everyone, I am developing a project using i.MX8MM. FPGA is required as an external memory device in the project, and Nandflash is also necessary.I read the entire manual carefully, and it seems that I did not find an EIM interface suitable for connecting to FPGA.Is there a good solution to this problem? 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,693件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi liaochao

 

one can consider other standard interfaces like flexspi, pcie, ecspi.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,677件の閲覧回数
chao
Contributor II

Thank you @igorpadykov  for the reply,

We have already used PCIe on other modules, so the PCIe interface cannot be used. In addition, ecspi cannot meet the communication bandwidth requirements.So flexspi may be the best choiAce. 

According to i.MX 8M Mini Applications Processor Reference Manual, Rev. 2, 08/2019, we did not find the specific details of how to communicate with FPGA. Do you have any application cases or  the information can be referenced.

 

0 件の賞賛
返信
3,674件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

for FlexSPI usage one can look at i.MXRT resources (it has the same module)

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-...

 

Best regards
igor

 

 

 

0 件の賞賛
返信
3,694件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi liaochao

 

one can consider other standard interfaces like flexspi, pcie, ecspi.

 

Best regards
igor

0 件の賞賛
返信