??? How to integrate M4 "hello-world" demo into secondary loader firmware using yocto?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

??? How to integrate M4 "hello-world" demo into secondary loader firmware using yocto?

667 Views
pavel_
Contributor II

Hello,

How to integrate M4 image containing for example a hello-world M4 demo into secondary loader firmware (imx-boot-imx8mmevk-sd.bin-flash_evk) in yocto?

We are using IMX8MMEVK

Labels (1)
0 Kudos
Reply
1 Reply

635 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pauli

could you please clarify task, do you mean "secondary firmware"

in sect.6.1.5.3.2 NAND flash boot flow ?

i.MX 8M Mini Applications Processor Reference Manual

This is used for primary and secondary boot images intended for A53 core,

not M4.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply