How to install linux for i.MX6 Board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to install linux for i.MX6 Board?

跳至解决方案
5,269 次查看
joowonkim
Contributor III

Hi everyone.

I want to install the linux on i.MX6 Board.

What need for install? and How to install linux for i.MX6?

please help

Thank you to read.

标签 (3)
1 解答
3,966 次查看
igorpadykov
NXP Employee
NXP Employee

H JooWon

you can two alternatives, first yocto (also please read attached Freescale_Yocto_Project_User's_Guide.pdf)

Yocto Training - HOME

L3.10.53_1.1.0_iMX6QDLS_Bundle : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation

second - ltib, for that first read below appnote

http://cache.freescale.com/files/dsp/doc/app_note/AN3875.pdf

the attached files

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
3,967 次查看
igorpadykov
NXP Employee
NXP Employee

H JooWon

you can two alternatives, first yocto (also please read attached Freescale_Yocto_Project_User's_Guide.pdf)

Yocto Training - HOME

L3.10.53_1.1.0_iMX6QDLS_Bundle : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation

second - ltib, for that first read below appnote

http://cache.freescale.com/files/dsp/doc/app_note/AN3875.pdf

the attached files

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,966 次查看
joowonkim
Contributor III

Hi igorpadykov

Thank you reply.

If install the linux on i.MX Board, could operating without SDcard?

thank you.

JooWon

0 项奖励
回复
3,966 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JooWon

SD is needed for rootfs, also one can use NAND or nfs instead SD.

Please read Linux User Guide for available options.

~igor

0 项奖励
回复