How to install & verify lpcscrypt in Ubuntu?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to install & verify lpcscrypt in Ubuntu?

1,298件の閲覧回数
GanesanGuru
Contributor IV

Hi fellas,

I've downloaded LPCScrypt v2.1.2 as lpcscrypt-2.1.2_57.x86_64.deb.bin and run with root privileges, yet I'm not sure where it has installed or how to access it further.. During installation, it happened as follows:

 

image.png

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,281件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which product are you using?

0 件の賞賛
返信

1,276件の閲覧回数
GanesanGuru
Contributor IV

Hi  @Rita_Wang   ,

I'm using iMX RT1064-EVK board and in order to re-program the onboard debugger LPC4322 using  AN13206 , I'm in need of the lpcsrypt . I'm installing those in Ubuntu OS and while installing I'm facing the issues mentioned above..

 

PS : I'm doing so, to program a custom board KM34 via this onboard debugger using LPC4322 MCU

0 件の賞賛
返信

1,273件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I create new case 00572365 to our RT engineer, she will give update to you then you will receive the email.