How to include x264enc to an image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to include x264enc to an image

跳至解决方案
2,250 次查看
philippeballeyd
Contributor IV

Hi

I just managed to bitbake the fsl-image-x11 image for the IMX6Q Sabre Board, and i'm now trying to use gstreamer to stream a webcam over the network.

It appears x264enc is not installed, so i tried to do it.

I tried multiple solutions found on the community forum ( Re: How to include x264enc on yocto and Task #9 - How to add bad/ugly ) but i'm getting the same error, for both solutions when using bitbake.

ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:

fatal: reference is not a tree: 585324fee380109acd9986388f857f413a60b896

ERROR: Logfile of failure stored in: /media/philippe/data/fsl-release-bsp/build-x11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/x264/r2265+gitAUTOINC+585324fee3-r0/temp/log.do_unpack.9681

Log data follows:

...

| DEBUG: Python function base_do_unpack finished

| DEBUG: Python function do_unpack finished

| ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:

| fatal: reference is not a tree: 585324fee380109acd9986388f857f413a60b896

|

ERROR: Task 4108 (/media/philippe/data/fsl-release-bsp/sources/poky/meta/recipes-multimedia/x264/x264_git.bb, do_unpack) failed with exit code '1'

Does anyone have an idea about this issue?

Thanks in advance.

标签 (3)
标记 (3)
1 解答
1,517 次查看
philippeballeyd
Contributor IV

Seems like the hash was incorrect, since they did tree maintenance.

Here's the one you should put in x264_git.bb : bfed708c5358a2b4ef65923fb0683cefa9184e6f

在原帖中查看解决方案

1 回复
1,518 次查看
philippeballeyd
Contributor IV

Seems like the hash was incorrect, since they did tree maintenance.

Here's the one you should put in x264_git.bb : bfed708c5358a2b4ef65923fb0683cefa9184e6f