Hi,
I want to implement a qt program including a window to play video using gstreamer. As I know the UI area above the video windows should be transparent.
Timesys theater system is a sample to do this. fb0 is qt program and fb2 is gstreamer video(mfw_v4lsink). But it only support global alpha and color key in fb0. I think I need to to pixel alpha which can then be supported by qt.
How can implement this function, should I shoud mfw_isink or I can implement with mfw_v4lsink.
Regards,
已解决! 转到解答。
Here is an example to config frame buffer for alpha in pixel function, you can have a try.
retval = ioctl(fd, FBIOGET_VSCREENINFO, &fb_var);
if (retval < 0)
{
printf("fb ioctl FBIOGET_VSCREENINFO fail\n");
}
fb_var.xres = 1280;
fb_var.yres = 720;
fb_var.bits_per_pixel = 32;
fb_var.activate |= FB_ACTIVATE_FORCE;
fb_var.nonstd = v4l2_fourcc('A', 'B', 'G', 'R');
fb_var.red.offset = 24;
fb_var.red.length = 8;
fb_var.green.offset = 16;
fb_var.green.length = 8;
fb_var.blue.offset = 8;
fb_var.blue.length = 8;
fb_var.transp.offset = 0;
fb_var.transp.length = 8;
fb_var.xres_virtual = fb_var.xres;
fb_var.yres_virtual = fb_var.yres * 3;
fb_var.yoffset = 0;
retval = ioctl(fd, FBIOPUT_VSCREENINFO, &fb_var);
if (retval < 0)
{
printf("fb ioctl FBIOPUT_VSCREENINFO fail\n");
}
loc_alpha.enable = 1;
loc_alpha.alpha_in_pixel = 1;
retval = ioctl(fd, MXCFB_SET_LOC_ALPHA, &loc_alpha);
if (retval < 0)
{
printf("fb ioctl MXCFB_SET_LOC_ALPHA fail\n");
}
ioctl(fd, MXCFB_WAIT_FOR_VSYNC, 0);
ioctl(fd, FBIOBLANK, FB_BLANK_UNBLANK);
Hi Ionsn,
I am trying to overlay 2D graphics on top of video output(using gstreamer). i went through this discussion and i have some queries:
1. Could you please help me to know what headers are required in the application because i am getting errors like:
error: 'MXCFB_SET_CLR_KEY' undeclared (first use in this function)
if ( ioctl(fd_fb, MXCFB_SET_CLR_KEY, &color_key) < 0) {
2. Should i write one single application for the video output and the 2D graphics overlayed or different applications?
Thanks in advance.
Now I can add local alpha with following code:
ioctl(fb0_fd, FBIOBLANK, FB_BLANK_NORMAL);
loc_alpha.enable = 1;
loc_alpha.alpha_in_pixel = 1;
result = ioctl(fb0_fd, MXCFB_SET_LOC_ALPHA, &loc_alpha);
if (result < 0)
{
printf("fb ioctl MXCFB_SET_LOC_ALPHA fail\n");
//goto err1;
}
ioctl(fb0_fd, MXCFB_WAIT_FOR_VSYNC, 0);
ioctl(fb0_fd, FBIOBLANK, FB_BLANK_UNBLANK)
But with this settings, I can only see the video and QT program at the same time in 16bpp mode(But the qt text above video is not very clear).
root@freescale ~$ fbset
mode "1280x720-60"
# D: 74.250 MHz, H: 45.000 kHz, V: 60.000 Hz
geometry 1280 720 1280 720 16
timings 13468 220 110 20 5 40 5
accel false
rgba 5/11,6/5,5/0,0/0
endmode
root@freescale ~$ fbset -fb /dev/fb2
mode "1280x720-54"
# D: 64.998 MHz, H: 40.624 kHz, V: 53.594 Hz
geometry 1280 720 1280 768 16
timings 15385 220 40 21 7 60 10
accel false
rgba 5/11,6/5,5/0,0/0
endmode
After I change the kernel command line to 32bpp:
console=ttymxc1,115200 video=mxcfb0:dev=hdmi,1280x720M@60,if=RGB24,bpp=32
or using fbset -depth 32,
then I can only see the QT graphic and I cann't see the video.
How can I make the correct settings to let QT and video be visible at the same time? I want to use QT widget's transparency to control the alpha effect.
Regards,
Here is an example to config frame buffer for alpha in pixel function, you can have a try.
retval = ioctl(fd, FBIOGET_VSCREENINFO, &fb_var);
if (retval < 0)
{
printf("fb ioctl FBIOGET_VSCREENINFO fail\n");
}
fb_var.xres = 1280;
fb_var.yres = 720;
fb_var.bits_per_pixel = 32;
fb_var.activate |= FB_ACTIVATE_FORCE;
fb_var.nonstd = v4l2_fourcc('A', 'B', 'G', 'R');
fb_var.red.offset = 24;
fb_var.red.length = 8;
fb_var.green.offset = 16;
fb_var.green.length = 8;
fb_var.blue.offset = 8;
fb_var.blue.length = 8;
fb_var.transp.offset = 0;
fb_var.transp.length = 8;
fb_var.xres_virtual = fb_var.xres;
fb_var.yres_virtual = fb_var.yres * 3;
fb_var.yoffset = 0;
retval = ioctl(fd, FBIOPUT_VSCREENINFO, &fb_var);
if (retval < 0)
{
printf("fb ioctl FBIOPUT_VSCREENINFO fail\n");
}
loc_alpha.enable = 1;
loc_alpha.alpha_in_pixel = 1;
retval = ioctl(fd, MXCFB_SET_LOC_ALPHA, &loc_alpha);
if (retval < 0)
{
printf("fb ioctl MXCFB_SET_LOC_ALPHA fail\n");
}
ioctl(fd, MXCFB_WAIT_FOR_VSYNC, 0);
ioctl(fd, FBIOBLANK, FB_BLANK_UNBLANK);