How to implement color key with IMX7 sabre board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to implement color key with IMX7 sabre board?

1,625 Views
mariuszpiotrows
Contributor I

How to implement color key with IMX7 sabre board?

Mentioned platform is lacking with IPU and graphic hardware acceleration (2D and 3D)

I was trying to do NXP test build in

example of PXP by running:

"root@imx7dsabresd:/unit_tests/Display# ./pxp_test.out -I "-h -v -l 10 -t 100"

---- Running < ./pxp_test.out > alloc_contig_range: [ac140, ac16b) PFNs busy
test ----

pxp_test.c:260 requested chan handle 0
pxp_test.c:360 opening this fb_dev - /dev/fb0
pxp_test.c:360 opening this fb_dev - /dev/fb1
pxp_test.c:360 opening this fb_dev - /dev/fb2
pxp_test.c:363 Unable to open /dev/fb2

----  Test < ./pxp_test.out > ended  ----"

it is failing and it is expecting "mxc_epdc_fb" if frame buffer id is different then I would failed,

Unfortunately I don't have EPDC interface connected,

I was able to modified /imx-test-5.9/test/pxp_lib_test/pxp_test.c file but it faild in two places:

ret = ioctl(fd_fb, FBIOPUT_VSCREENINFO, &var); // this could be omitted
retval = ioctl(fd_fb, MXCFB_SEND_UPDATE, &upd_data); // always failed

Any advice how to implement color keying with IMX7D sabre board ?

Labels (4)
Tags (1)
0 Kudos
Reply
2 Replies

1,335 Views
mariuszpiotrows
Contributor I

Hello,

Thank you for replay,

I am not using EPDC, is the PXP only working with EPDC

or is going to work with LCD?

 

I do care about color keying or other way to overlay graphics(GUI) on top of Video which come from gStreamer 

Is this possible with IMX7 when there is no IPU ?

If it is possible how to do it ?

Regards,

0 Kudos
Reply

1,335 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Mariusz

You need to enable PXP driver for EPDC on i.MX 7Dual, is the only way. However due lack of IPU the color key is not going to work.

Regards

0 Kudos
Reply