How to implement DFU in IMX RT1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to implement DFU in IMX RT1170

跳至解决方案
1,382 次查看
Ragnar
Contributor III

Hello,

         I want to update the IMX RT1170 firmware through the DFU via USB.

I have gone through the basic USB examples provided in the SDK. There I found examples regarding the DFU "evkmimxrt1170_dev_dfu_freertos_cm7". But in those I didn't find any text documents that explains how to executive it like other examples has.

I want to know the following:

1. Does the DFU works with the J11(On board debugger) or else I have to use the OTG's provided.

   If it works with the J11. How it would be and can I use the J11 for Debugging and DFU at the same time.

2. Is there any application that can supports for DFU on windows to update the RT1170 firmware through USB.

DFU example:

Ragnar_0-1702625025040.png

 

HID example:

Ragnar_1-1702625107144.png

 

          Thanks & Regards,

             Ragnar.

0 项奖励
回复
1 解答
1,362 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Ragnar,

The evkmimxrt1170_dev_dfu_freertos_cm7 example code does have a readme file, it is just a bit more tricky to find it. You need to navigate to the SDK installation path, by default it is: C:\Users\<user>\mcuxpresso\02\SDKPackages\

In there, extract the SDK, and follow this path: SDK_2_14_0_MIMXRT1170-EVKB.zip\boards\evkbmimxrt1170\usb_examples\usb_device_dfu\freertos\cm7

Here you will find the readme.pdf, which is a 12 page pdf that has all of the information and explains all of the setup and process for the usb dfu example code.

I hope this helps!

BR,
Edwin.

在原帖中查看解决方案

2 回复数
1,357 次查看
Ragnar
Contributor III

Hi @EdwinHz,

           Thanks for the reply. 

           Now, I was able to execute the given SDK example.

           Thanks & Regards,

                Ragnar.

     

 

0 项奖励
回复
1,363 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Ragnar,

The evkmimxrt1170_dev_dfu_freertos_cm7 example code does have a readme file, it is just a bit more tricky to find it. You need to navigate to the SDK installation path, by default it is: C:\Users\<user>\mcuxpresso\02\SDKPackages\

In there, extract the SDK, and follow this path: SDK_2_14_0_MIMXRT1170-EVKB.zip\boards\evkbmimxrt1170\usb_examples\usb_device_dfu\freertos\cm7

Here you will find the readme.pdf, which is a 12 page pdf that has all of the information and explains all of the setup and process for the usb dfu example code.

I hope this helps!

BR,
Edwin.