How to get the load of each core for i.mx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get the load of each core for i.mx6q

Jump to solution
1,416 Views
宗標廖
Contributor V

Hello Community

As we know,there are four cores for i.mx6q,so could you tell me how to get the load of each core.

#top command cannot do this.

Best Regards,

ZongbiaoLiao

Labels (2)
0 Kudos
Reply
1 Solution
1,290 Views
宗標廖
Contributor V

I find the answer at

Re: load per cpu

thank you!

View solution in original post

0 Kudos
Reply
2 Replies
1,291 Views
宗標廖
Contributor V

I find the answer at

Re: load per cpu

thank you!

0 Kudos
Reply
1,290 Views
b36401
NXP Employee
NXP Employee

Hello,

Yes. You can type "1" when you are running top utility to see per core CPU load.

Have a great day,
Victor

0 Kudos
Reply