How to get the IMX6Q's Fcanclk frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to get the IMX6Q's Fcanclk frequency

跳至解决方案
1,038 次查看
jiongzhongliu
Contributor III

The IMX6Q's datasheet describe that the "Ftq = Fcanclk/prescaler", the problem is that how can I know or calculate the Fcanclk? I need to know the Fcanclk value, because I develop the IMX6Q on a bare board.Is anybody know it?

标签 (1)
0 项奖励
回复
1 解答
949 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jiongzhong

please check description in sect.26.8.13 Control 2 Register (FLEXCANx_CTRL2)

http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf :

fCANCLK is the Protocol Engine (PE) Clock in Hz; PE clock is derrived from

CAN_CLK_ROOT in CCM. See Clock Root Generator, sect.18.5.1.5.4 Clock Root Generator,

from Table 26-2. FLEXCAN Clocks : Protocol Engine clock is can_clk_root

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
950 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jiongzhong

please check description in sect.26.8.13 Control 2 Register (FLEXCANx_CTRL2)

http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf :

fCANCLK is the Protocol Engine (PE) Clock in Hz; PE clock is derrived from

CAN_CLK_ROOT in CCM. See Clock Root Generator, sect.18.5.1.5.4 Clock Root Generator,

from Table 26-2. FLEXCAN Clocks : Protocol Engine clock is can_clk_root

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------