How to get protobufs and zeromq included in Yocto image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get protobufs and zeromq included in Yocto image

3,354件の閲覧回数
stephen_eng
Contributor III

I want to use zeromq and google protobuf for my application. From what I can tell, it looks like the 4.14.78_1.0.0 sumo Yocto build should have a version of zeromq included as part of meta-oe, but I can’t seem to find it anywhere in the image. (No library, no files with zeromq or zmq in the name.) I’m wondering if the default build somehow removed it, or if I need to do something else to ensure that it’s included in the image.

 

For protobufs, it looks like it’s not there at all… I tried to use devtool to create a ‘protobuf’ recipe, but it fails to build.

 

Is there another way of adding protobufs to my project?

 

I’m just going for the fastest path forward. If there’s already a layer that exists for one or both of these components, or a recipe, or something… I would appreciate that.

 

Thanks,

0 件の賞賛
4 返答(返信)

3,201件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛

3,201件の閲覧回数
stephen_eng
Contributor III

Just to check that I understand you.

I would have to add the devtools recipe from the meta-virtualization layer to my image, and make sure those 3 things build?

Is there a spot for zeromq as well? (I plan to use it with Python, if that helps narrow what I need to incorporate.)

0 件の賞賛

3,201件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi, There is no Spot for zeromq you have to change all the register to support it.

Regards

0 件の賞賛

3,201件の閲覧回数
stephen_eng
Contributor III

It looks like I have zeromq support via Python. (python-pyzmq package is available) I was able to add it to my image, and verify that it connects to my host machine.

0 件の賞賛