How to get i.MX6SL BSP L3.0.35_2.1.0_130506_source.tar.gz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get i.MX6SL BSP L3.0.35_2.1.0_130506_source.tar.gz

364 Views
洲邓
Contributor II

Hi expert,

请问是否可以提供 i.MX6SL 的L3.0.35_2.1.0_130506_source.tar.gz这个BSP 包,

http://www.freescale.com/zh-Hans/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&fpsp=1&tab=Design_Too...

中只有L3.0.101_4.1.1_141016_source.tar这个版本,如何能够获取到L3.0.35_2.1.0_130506_source.tar.gz 呢?

thanks

BR,

Dany

Labels (1)
0 Kudos
1 Reply

308 Views
igorpadykov
NXP Employee
NXP Employee

Hi 洲 邓

L3.0.35_2.1.0_130506_source.tar.gz is old release and was removed

from public web page. You can enter support ticket and obtain link from

internal FSL server.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos