How to get gcc-4.6.2-glibc-2.13-linaro-multilib

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get gcc-4.6.2-glibc-2.13-linaro-multilib

6,324 次查看
Joerg-SH
Contributor III

I found a lot of How To witch use that but how to get it????

Thanks in advance

Joerg

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

2,926 次查看
gusarambula
NXP TechSupport
NXP TechSupport

The GCC Linaro 4.6.2 Multilib Toolchain is included in Freescale’s Linux BSP, available for download at Freescale.com

Let me know if you have trouble finding it and also let me know which i.MX processor you’re using. The version of toolchain you mentioned is currently tested on i.MX6.

0 项奖励
回复

2,926 次查看
dionisiocarvalh
Contributor I

Hi gusarambula,

I have the same issue to get the gcc.

I didn't found it on Freescale site.

Can you help me?

My processor is the QMX6 ( PN016101)

Thanks a lot.

Best Regards

Att

Dionisio

0 项奖励
回复

2,926 次查看
gusarambula
NXP TechSupport
NXP TechSupport

The toolchain is available as part of the Freescale Linux BSP. This BSP only supports our boards but you may find it useful for extracting the toolchain. The BSPs are available on the Software & Tools section of each i.MX processor.

Go to  freescale.com/imx6

Then chose the i.MX6 processor you’ll be using, for example i.MX6Q.

Once on the i.MX6Q page go to to the Software & Tools tab and look under the Run-time Software -> Operating System Software-Board Support Packages section.

In your particular scenario, the board you’re using is from Adeneo, their BSP are available here, although the source code is moderated but you may contact them for more information on how to get it:

http://www.adeneo-embedded.com/Products/Board-Support-Packages/Congatec-conga-QMX6-BSPs

0 项奖励
回复

2,926 次查看
satoshishimoda
Senior Contributor I

Hi gusarambula,

I found gcc-4.6.2-glibc-2.13-linaro-multilib binary file in /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin.

However, I did not find the source codes of it.

Would you let me know where are the source codes of gcc-4.6.2-glibc-2.13-linaro-multilib?

Best Regards,

Satoshi Shimoda

0 项奖励
回复