How to get camera RAW data in i.MX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get camera RAW data in i.MX8

717件の閲覧回数
xu_ji1
Contributor V

Hello,

I used max9286 and camera is mono Raw 12bit output and max9286 also use Raw12 output to CSI,

How can I get the Raw data max9286 output?

I used application get camera data set format V4L2_PIX_FMT_Y16,why it happened VIDIOC_S_FMT failed?

does i.MX8 not support this format?

Thanks

ラベル(1)
2 返答(返信)

573件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xu

yes ISI supports that format, unfortunately linux software seems not support yet.

For help one can apply to Commercial Support and Engineering Services | NXP 

or try to convert to other formats using Soft ISP :

https://www.nxp.com/docs/en/application-note/AN12060.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

573件の閲覧回数
xu_ji1
Contributor V

Hi,

And how can I dump camera Raw data?

Thanks

0 件の賞賛
返信