How to get Vivante GC2000 drivers for armhf linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to get Vivante GC2000 drivers for armhf linux

跳至解决方案
1,821 次查看
buddhikedesilva
Contributor II

Are these drivers including x11 available for download?

标记 (2)
1 解答
1,022 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Buddhike

please look at libs imx-gpu-viv-5.0.11.xx-hfp.bin

meta-fsl-arm - Layer containing Freescale ARM hardware support metadata

and BSP package

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
1,023 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Buddhike

please look at libs imx-gpu-viv-5.0.11.xx-hfp.bin

meta-fsl-arm - Layer containing Freescale ARM hardware support metadata

and BSP package

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,022 次查看
buddhikedesilva
Contributor II

Thanks Igor. I will try them out.

0 项奖励
1,022 次查看
buddhikedesilva
Contributor II

Hi Igor.

I'm using Yocto now. Do you know which recipe I could use to generate X11 with vivante drivers?

Thanks,

Buddhike

0 项奖励
1,022 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Buddhike

please look at Table 1. Freescale Yocto project images

Freescale_Yocto_Project_User's_Guide.pdf included in

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

~igor

0 项奖励