How to flash u-boot.bin to NAND Flash on IMX6Q_SabreAI board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to flash u-boot.bin to NAND Flash on IMX6Q_SabreAI board.

863 Views
chamansaurav
Contributor I

I tried Nand write command of u-boot to flash u-boot image on the NAND chip.

But, it did not work.

I am looking for MFG_tool which can flash u-boot.bin to NAND.

In the document i.MX 6Dual/6Quad SABRE-AI Linux User's Guide it says to use Mfgtools-Rel-4.0.0_130424_MX6Q_UPDATER.tar.gz.

My question is where can i download this Mfgtools-Rel-4.0.0_130424_MX6Q_UPDATER.tar.gz.

Or any MfgTool can be used to download boot images on this board.

Labels (1)
0 Kudos
Reply
2 Replies

540 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Chaman Saurav,

Here you can use the mfgtool to download the images to nand on your board. Here could you tell me which version BSP are you using?
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

540 Views
chamansaurav
Contributor I

Hi Rita

I am using L3.0.35_4.1.0_130816_source BSP.

I used LTIB to build images.

I need to flash u-boot image to the NAND chip.

Which MfgTool I should use?

From where can I download the same?

Regards

Chaman

0 Kudos
Reply