How to flash the UUC software over the NAND Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to flash the UUC software over the NAND Flash

3,262 Views
adityanagal
Contributor III

HI ,

I am working over the IMX6 solo based target board , where the raw Nand Flash is used as the booting device. As per discussion in the below thread. UUC software need to be written over the Nand Flash so it can take commands from MfgTool. UUC software is used for flashing the Nand Flash. My question is , how to flash the UUC software to Nand Flash. Please suggest.

Regards,

Aditya Nagal

0 Kudos
Reply
4 Replies

3,093 Views
xixiguohan
Contributor II

Hi Aditya

Do you solve the problem? Can you show me your method?

Best Reagrds

xixiguo

0 Kudos
Reply

3,090 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

for UUC details please refer to p.4 attached document from

MFG Tools documentation. In latest MFG Tools yocto releases

it is generated using commands described in sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,090 Views
xixiguohan
Contributor II

Hi igor

Add new configuration file in config\platform\imx, such as mx6q_arm2_mfg_config.

what directory does config\platform\imx belong to? uboot? kernel?

Best Regards

xixiguo

0 Kudos
Reply

3,090 Views
igorpadykov
NXP Employee
NXP Employee

Hi xixiguo

this is for ltib, for yocto please follow Yocto Guide.

Best regards
igor

0 Kudos
Reply