How to flash secondary bootlaoder(uboot) on the IMX6Q/DL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash secondary bootlaoder(uboot) on the IMX6Q/DL.

1,752件の閲覧回数
sumanthgavini
Contributor I

Details: 

Processor:  IMX6Dual

disk : SSD (solid state disk)  --- sata type(Installing Android OS on SSD device). 

OS : Android 6.0

uboot version: 2015.04-00001

kernel version : 3.14.52 

At present flashing the uboot through the MFG tools: 

i.e  dd if=$FILE of=/dev/sda bs=512 seek=2 skip=0 conv=fsync">write U-Boot to sata</CMD>

1. How to configure Redundant boot support for SSD? 

2. How to test/verify Redundant boot support for SSD?

3. Do I need to configure HAB to support redundant boot support, if So how to configure HAB for IMX6DL?

3. Does, i need to authenticate the uboot.bin with  HAB signing tool to redundant boot support? 

Regards,

Sumanth. 

ラベル(6)
0 件の賞賛
返信
2 返答(返信)

1,492件の閲覧回数
sumanthgavini
Contributor I

ShaojunWang‌   alejandrolozanoYuriMuhin_ngart‌  Can you help on this? 

0 件の賞賛
返信

1,492件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize for the late answer.

In the below document, you can see how to boot a Linux image from SATA drive.

Booting Linux from SATA on i.MX6Q SABRE AI. 

For Android can be similar, the difference can that you need to save your u-boot image in your SD card or your e-mmc and the remaining images can be saved in your SSD disk.

Hope this can help you.

Best Regards,

Diego.

0 件の賞賛
返信