How to fix tpm2-tool issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to fix tpm2-tool issue

1,614 Views
t2865k5
Contributor I

Dear NXP ,

HW : srg-imx8mplus

repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-langdale -m imx-6.1.1-1.0.1.xml

(1) I use imx8mplus + Debian 11 OS .  Run command as follows :

tpm2_selftest

tpm2_getcap properties-fixed

test result :

 

TPM2_PT_FAMILY_INDICATOR:

  raw: 0x322E3000

  value: "2.0"

TPM2_PT_LEVEL:

  raw: 0

TPM2_PT_REVISION:

  value: 1.38

......

........

Kernel image and device tree settings are correct. 

(2) I use imx8mplus SDK to run bitbake imx-image-full command. 

Run tpm2_selftest command . Please refer to the following pictures .

 

t2865k5_0-1698222539357.png

t2865k5_1-1698222651987.pngt2865k5_2-1698222698902.png

 

Could you tell me how to fix this issue .

 

 

 

 

 

 

 

 

0 Kudos
Reply
2 Replies

1,585 Views
t2865k5
Contributor I

Dear NXP ,

Use bitbake imx-image-full to build image . It include a tpm2-tools . Is there any difference between it and github tpm2-tools?

 

0 Kudos
Reply

1,600 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

This is one of Yocto package, please download all the package yocto need before build the image:

https://github.com/tpm2-software/tpm2-tools

 

Regards

0 Kudos
Reply