How to enable the EPIT for imx6 solo x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable the EPIT for imx6 solo x

27,335件の閲覧回数
ravis5354
Contributor I

Hi All. I am trying to use EPIT. I have made some changes on below file.

imx6sx.dtsi -  >  

epit1: epit@020d0000 {

compatible = "fsl,imx6sx-epit", "fsl,imx31-epit";

reg = <0x020d0000 0x4000>; 

interrupts = <GIC_SPI 56 IRQ_TYPE_LEVEL_HIGH>;

clocks = <&clks IMX6SX_CLK_EPIT1>;

clock-names = "ipg", "per";

status = "okay";

};

epit2: epit@020d4000 {

compatible = "fsl,imx6sx-epit", "fsl,imx31-epit";

reg = <0x020d4000 0x4000>; 

interrupts = <GIC_SPI 57 IRQ_TYPE_LEVEL_HIGH>;

clocks = <&clks IMX6SX_CLK_EPIT2>;

clock-names = "ipg", "per";

status = "okay";

};

2- Please find the attached simple epit module.

3 - When I am inserting the module getting below error

" EPIT1 base address: c0dc0000
genirq: Flags mismatch irq 56. 00000004 (EPIT1) vs. 00000004 (sdma)
EPIT1 request_irq return -16
EPIT1 : request_irq() failure! ""

Can you please help me how to resolve this error.

 

Thanks in advance.

0 件の賞賛
返信
1 返信

27,326件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

Please refer to the Linux Reference Manual, available in the following link => Supporting information => Linux docs: https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

There you will find information about the timer (chapter 2.1.3) and the files available to set it. Additionally, you can refer to the i.MX6 Solo X Reference Manual, chapter 25 for more information about the EPIT: https://www.nxp.com/webapp/Download?colCode=IMX6SXRM

 

Hope it helps!

 

BR,

Ivan.

0 件の賞賛
返信