How to enable power key long press boot sequence on i.MX6 ULL + evk board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable power key long press boot sequence on i.MX6 ULL + evk board?

1,524 Views
alleenwang
Contributor II

Hi guys,

We plan to use i.MX6 ULL and evk board for our product prototype.

MCIMX6ULL-EVK|i.MX6ULL Evaluation Kit|NXP 

Our product had 1 request was long press power key and boot-up device.

But, when we use i.MX6ULL and evk board, it will auto boot-up when connects the DC power.

Why evk board does not need to press the power key for device boot-up ?

How to enable this feature ? (Or re-work evk board ?)

Labels (4)
0 Kudos
Reply
1 Reply

1,198 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alleen

one can try solution provided for turning on pmic on i.MX6Q Sabre SD

schematic spf-27392 p.19 "OPTIONAL PMIC POWER.."

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES

SABRE Platform for Smart Devices|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply