Hi,
I'm using imx8m custom board, linux 4.9.51 ga release.
I'm trying to implement QSPI_A and QSPI_B in imx8m platform. I'm able to add QSPI_A(alone) successfully. If I add both QSPI_A and B, the board hangs. If I try to add QSPI_B alone by disabling A, I get the below messages:
=======================================================
# dmesg | grep -i spi
fsl-quadspi 30bb0000.qspi: unrecognized JEDEC id bytes: 00, 00, 00
fsl-quadspi 30bb0000.qspi: Freescale QuadSPI probe failed
fsl-quadspi: probe of 30bb0000.qspi failed with error -2
========================================================
Following is the dts node and pin controls I'm using.
&qspi {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_qspi>;
status = "okay";
flash0: mt25qu256aba@0 {
reg = <0>;
#address-cells = <1>;
#size-cells = <1>;
compatible = "micron,mt25qu256aba";
spi-tx-bus-width = <4>;
spi-rx-bus-width = <4>;
spi-max-frequency = <12000000>;
spi-nor,ddr-quad-read-dummy = <6>;
status="okay";
};
flash1: mt25qu256aba@1 {
reg = <1>;
#address-cells = <1>;
#size-cells = <1>;
compatible = "micron,mt25qu256aba";
spi-tx-bus-width = <4>;
spi-rx-bus-width = <4>;
spi-max-frequency = <12000000>;
spi-nor,ddr-quad-read-dummy = <6>;
status = "okay";
};
};
....
pinctrl_qspi: qspigrp {
fsl,pins = <
MX8MQ_IOMUXC_NAND_ALE_QSPI_A_SCLK 0x82
MX8MQ_IOMUXC_NAND_CE0_B_QSPI_A_SS0_B 0x82
MX8MQ_IOMUXC_NAND_DATA00_QSPI_A_DATA0 0x82
MX8MQ_IOMUXC_NAND_DATA01_QSPI_A_DATA1 0x82
MX8MQ_IOMUXC_NAND_DATA02_QSPI_A_DATA2 0x82
MX8MQ_IOMUXC_NAND_DATA03_QSPI_A_DATA3 0x82
MX8MQ_IOMUXC_NAND_CLE_QSPI_B_SCLK 0x82
MX8MQ_IOMUXC_NAND_DATA04_QSPI_B_DATA0 0x82
MX8MQ_IOMUXC_NAND_DATA05_QSPI_B_DATA1 0x82
MX8MQ_IOMUXC_NAND_CE2_B_QSPI_B_SS0_B 0x82
MX8MQ_IOMUXC_NAND_DATA06_QSPI_B_DATA2 0x82
MX8MQ_IOMUXC_NAND_DATA07_QSPI_B_DATA3 0x82
>;
};
Is this correct? There is no clock when I probe. Is there anything which is needed to be added to enable QSPI_B apart from the dts?
Thanks in advance.
Regards,
Prajna