Hello,
I am using Yocto to build Linux image to run on IMX8M-MINI based DART-MX8M-MINI SOC ,on VAR-DT8M Board.
I booted the board with the fsl-image-gui image copied on SD card, and from log I doubt it is bringing up the PCIe bus.
The build procedure I am following the doc setup guide , and I didn't apply any changes on the Yocto project.
I haven't connected and mini PCIe device but wanted to know from the boot log i received if that is what is expected and if the bus is enabled, the CONFIG parameters for PCI in my dts file seems to be enabled.The boot log I received is:
root@imx8mm-var-dart:~# dmesg | grep -i pci
[ 0.522332] PCI: CLS 0 bytes, default 64
[ 1.768407] imx6q-pcie 33800000.pcie: 33800000.pcie supply epdev_on not found
[ 1.785835] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 range:
[ 1.799468] imx6q-pcie 33800000.pcie: IO 0x1ff80000..0x1ff8ffff -> 0x00000
[ 1.814603] imx6q-pcie 33800000.pcie: MEM 0x18000000..0x1fefffff -> 0x18000
[ 1.829011] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.952987] imx6q-pcie 33800000.pcie: Phy link never came up
[ 2.958688] imx6q-pcie 33800000.pcie: failed to initialize host
[ 2.964634] imx6q-pcie 33800000.pcie: unable to add pcie port.
已解决! 转到解答。
Hi bhabu_bindu
seems it is enabled, for testing recommended to attach some pcie card, just for reference dts file:
Best regards
igor
Hi bhabu_bindu
seems it is enabled, for testing recommended to attach some pcie card, just for reference dts file:
Best regards
igor