How to enable LVDS-HDMI on imx8quadxplus evk kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable LVDS-HDMI on imx8quadxplus evk kit

2,562 Views
hemanthemb
Contributor I

Hi @nxp ,

we are using IMX8Quadxplus-mek evaluation kit with custoom Yocto image ,we want to use Lvds-hdmi bridge adapter in that board but during checking we identified 

[    3.257459] it6263 17-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[    3.369227] it6263 18-004c: Probe failed. Remote port 'lvds-channel@0' disabled

so to avoid this to enable the the Lvds-hdmi which device tree file need to modify can you please help this out.

Thanks in Advance,

hemanthemd.

 

 

0 Kudos
Reply
11 Replies

2,538 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Please connect the LVDS-HDMI card in LVDS0 connector as is in the next image:

JorgeCas_0-1733414696204.png

Then you need to use imx8qxp-mek.dtb device tree.

Set the U-Boot environment variable to imx8qxp-mek.dtb

=> setenv fdtfile imx8qxp-mek.dtb
=> saveenv
=> boot

Best regards.

0 Kudos
Reply

2,411 Views
hemanthemb
Contributor I

Hi @JorgeCas , @nxp
Thanks for the reply.
Media.jpg

 

we followed the same procedure 

setenv fdtfile imx8qxp-mek.dtb
=> saveenv
=> boot

but we are getting the error as I attached. kindly assist us to enable LVDS-HDMI via IT6263 driver it's a priority task Media (1).jpg

 

0 Kudos
Reply

2,401 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It is working as expected in my side, please try to re-flash the image and test again.

JorgeCas_0-1733940490574.jpeg

Best regards.

2,380 Views
hemanthemb
Contributor I
Hi,
thanks for the positive reply,
are you using custom yocto for the board or pre built image
kindly share the image or (.dtb files) or local.conf or major change where we need to do just assist us to test the same with our hardware hope will share the positive info.

thanks.
0 Kudos
Reply

2,366 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I used the pre-built image, and I didn't do any change, the device tree by default is imx8qxp-mek.dtb

Best regards.

0 Kudos
Reply

2,362 Views
hemanthemb
Contributor I
hi,
can you share the defualt image which will be very helpful for us.

thanks
0 Kudos
Reply

2,359 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I used this image:

Embedded Linux for i.MX Applications Processors | NXP Semiconductors

It seems that there is an issue in the page, it should be solved soon.

JorgeCas_0-1734018919588.png

And the command in UUU to flash it was:

uuu uuu.auto

Best regards.

 

0 Kudos
Reply

2,355 Views
hemanthemb
Contributor I
Hi,
first of all thanks for the quick reply,
i will check that
request:if you have local dowbload kindly share and what challanges you faced if any ruff note attach that too ,
this will be very helpful.
thanks
0 Kudos
Reply

2,307 Views
hemanthemb
Contributor I
Hi,
The imx8qxplus-mek.dtb file which you used can you share that it will be useful.
and with that any challenges faced that also kindly let us know if its possible to share the process(Image).
Thanks.
0 Kudos
Reply

2,295 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You need to download it from the website, I cannot share it.

Best regards.

0 Kudos
Reply

2,144 Views
hemanthemb
Contributor I
Hi @JorgeCas,@nxp

we followed the same image which you referred from the nxp site but still we are facing same issue even though we used fdt_file as imx8qxp-mek.dtb but for you as mentioned its working fine without any modifications.

but can you confirm is your board imx8quadxplus -mek kit and used image was same like downloaded from nxp site and have you done anything  to enable lvds-hdmi(it6263 driver) becuase in your setup hdmi moniter is working and up.

becuase we are facing same errors which i attached in our previous chat like so can you assist us to overcome .
0 Kudos
Reply