How to enable IPU with LCD QVGA TFT in iMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable IPU with LCD QVGA TFT in iMX6

2,757 次查看
ducminhnguyen
Contributor I

Hi everyone,

I am a student and now I have a project with iMX6S5 custom board and bare metal code from SDK 1.1. I try to setup and run simulation IPU with one TFT LCD QVGA 320x240 by RGB interface but not yet successful and I have some trouble:

- In file ipu_dc.c

If I enable PROG_CHAN_TYP to avoid image tearing as in the SDK:

      ipu_write_field(ipu_index, IPU_DC_WR_CH_CONF_5__PROG_CHAN_TYP_5, 4);

the function " ipu_enable_display(int32_t ipu_index) " can not call and I get error about memory fail to access and get stuck at IPU_IPU_CONF__DC_EN.

So if I disable it by write 0, ipu can enable but the screen is totally white and there is no Freescale Logo here.

- For RGB interface, do I really need the DRDY because my hardware the DI0_PIN15 is not connect with LCD.

I think maybe I make something wrong. I build the project in Eclipse with GNU ARM Toolchain then debug with Segger JLink under U-boot, program is loaded into RAM. Setting for my LCD is:

 

"Ampire QVGA", // name
Ampire_QVGA, // panel id flag
DISP_DEV_TFTLCD, // panel type
DCMAP_RGB666, // data format for panel
60, // refresh rate
320, // panel width
240, //panel height
6500000, // pixel clock frequency
93, // hsync start width
25, // hsync width
20, // hsyn back width
28, // vysnc start width
10, // vsync width
4, // vsync back width
0, // delay from hsync to vsync
0, // interlaced mode
0, // clock selection, internal
0, // clock polarity
0, // hsync polarity
0, // vync polarity
1, // drdy polarity
0, // data polarity

Other things I keep same as in the SDK 1.1.

Thanks and Best Regards.

标签 (5)
0 项奖励
回复
2 回复数

2,370 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Duc

please try to run sdk examples using sect.5 How to run a test

attached document. As for uboot lcd integration, please try patches on

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,370 次查看
ducminhnguyen
Contributor I

Hi Igor,

Thanks for your support.

I tried all the way but the screen is just white. I just want to implement the bare metal code and develop firmware for the custom board.

I think there is no output from RGB interface (DISP0_DATA0 ... DISP0_DATA23) to the LCD or maybe no data transfered from memory. For testing I just built with Plartform Init, PWM for the LCD backlight and IPU module.

Do I need to include other blocks in SDK folder?

For the LCD, if the DRDY is not connect between LCD and Board, is there possible for me to connect synchronous RGB interface for LCD?

I hope that you can help me soon.

Thanks and Best Regards,

Nguyen.

0 项奖励
回复