How to enable I-cache and D-cache on i.MX1060 and i.MX1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to enable I-cache and D-cache on i.MX1060 and i.MX1170

跳至解决方案
1,451 次查看
kenji
Contributor IV

Hi Team

 

How to enable I-cache and D-cache on i.MX1060 and i.MX1170?
I looked processor reference manual and AN12077, but I don't know how to set.

  1. Any documents or sample code for it is available?
    I would like sample code.
  2. Can it be set with MCUXpresso Config Tools  (like STM32CubeIDE )?
  3. Does the TCM memory controller have fast mode enabled as the default setting?

-----------------------

Really NXP documents is hard to read. The sentences are uselessly long and information is also lacking. It's hard to find what want to know.

Of course not perfect, but TI, Microchip and ST Micro documents are well organized and easy to read. Supplementary materials are also substantial.

I hope it will be improved.

 

 

标记 (2)
0 项奖励
回复
1 解答
1,438 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Kenji,

  1. You can refer to this appnote: https://www.nxp.com/docs/en/application-note/AN12042.pdf SDK drivers and CMSIS cache functions are mentioned in this document.
  2. No, unfortunately cache cannot be configured with MCUXpresso Config Tools.
  3. Yes.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,439 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Kenji,

  1. You can refer to this appnote: https://www.nxp.com/docs/en/application-note/AN12042.pdf SDK drivers and CMSIS cache functions are mentioned in this document.
  2. No, unfortunately cache cannot be configured with MCUXpresso Config Tools.
  3. Yes.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 项奖励
回复
1,422 次查看
kenji
Contributor IV

Hi @FelipeGarcia -san

The app note helps me, thank you!

And, it is difficult to find the desired documents on NXP website.
I hope it will be improved.

标记 (2)
0 项奖励
回复