How to enable GPU and check GPU utilization on i.MX6Q?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable GPU and check GPU utilization on i.MX6Q?

4,462 次查看
ponguru_s
Contributor III

I'm using i.MX6q board with Yocto 4.1.15-2.0.0. I want to enable GPU acceleration on the board. Also, I want test the GPU utilization just like 'free' command to check RAM utilization.

I need some examples to compare the graphics.

Igor1z

标记 (1)
2 回复数

2,822 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Surendranath

please use nxp bsps on below link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

and enable gpu driver described in Linux Manual included in Doc package:

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

also one can use

 IDE - Debug, Compile and Build Tools (15)
i.MX6D/Q/DL/S/SX GPU Tools
http://www.nxp.com/products/microcontrollers-and-processors/arm-based-portfolio/i.mx-applications-pr...

utilization can be checked with top command.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,822 次查看
ponguru_s
Contributor III

Thank you for the reply.

0 项奖励
回复