How to enable CRC image check at bootup for MIMXRT685?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable CRC image check at bootup for MIMXRT685?

651 Views
pcpro1789
Contributor III

To enable CRC image check at bootup for MIMXRT685 is it just a matter of following the CRC example in the SDK or is there something more integrated?

Tags (3)
0 Kudos
Reply
2 Replies

612 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can check the checksum of the CRC but will have to work with the example demo in the SDK.

https://mcuoneclipse.com/2018/03/05/tutorial-crc32-checksum-with-the-kboot-bootloader/

 

Regards

0 Kudos
Reply

578 Views
pcpro1789
Contributor III
Is there a bootloader configuration tool for the MIMXRT685, similar to the Kinetis Bootloader Configuration utilty?
0 Kudos
Reply
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----