How to enable A7 LDO?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable A7 LDO?

3,710件の閲覧回数
stanley_yeh
Contributor II

Hi,

I am using i.MX7ULP now and I want to enable A7 LDO.

I got some clues in 36.2.3.1 of IMX7ULPRMV2_RevC.pdf.

However, I don't know how to modify the parameter (please refer to the following image) of eFuse.

As I know, once the parameter be enabled, M4 will set PMC_0_CTRL[LDOEN] bit and the current of A7 domain will be from the internal LDO. Isn't it?

In addition, I can't find "fuse map" in the document as well.

Could you help me, please?

Image 11.png

ラベル(1)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

3,599件の閲覧回数
stanley_yeh
Contributor II

Hi igorpadykov,

Thank you for your help.

In addition, if I want to set the "A7 LDO Enable" bit as 1, which value of u-boot command is correct?

A. fuse prog 2 3 0x00000001

B. fuse prog 2 3 0x01000000

Thanks a lot.

pastedImage_1.png

0 件の賞賛
返信

3,599件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stanley

 for fuses programming one can look on

Burning eFuses on i.MX6 and i.MX7 - i.MXDev Blog 

Best regards
igor

0 件の賞賛
返信

3,599件の閲覧回数
stanley_yeh
Contributor II

Hi igorpadykov,

I know how to program.

What I don't know is the address order, little-endian or big-endian?

In the Bank 2 Word 3, the byte order is "0x530 0x531 0x532 0x533" or "0x533 0x532 0x531 0x530"?

If I want to set the "A7 LDO Enable" bit as 1, which value of u-boot command is correct? 0x00000001 or 0x01000000?

Thanks.

0 件の賞賛
返信

3,598件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stanley

fuse map can be found in attachment section of Reference Manual,

also attached below.

i.MX 7ULP Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信