I connect pannel direct to LVDS1, run and run android in xen mode. how to fix display it6263 bridge to direct LVDS panel?
how to fix the part of "passthough" ?
Hi wanben
one can try with below dts
imx8qm-mek-domu.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel
and follow sect.11 Xen Linux Guide in Linux 5.4.3_1.0.0 Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I think flowing:
1. Not design in my own board, my board is LVDS connect to panel direct, how to replace it6263 with panel mode. I found source code flowing file, have any change example?
~/mx8/yocto/android_build/vendor/nxp/mcu-sdk-auto/SDK_MEK-MIMX8QM/boards/mekmimx8qm/demo_apps/rear_view_camera/cm4_core1/isi_board.c
2. How to fix the part of "passthough", my board is without it6263, is panel !
Technically this is not xen specific. Put your node under passthrough, see if it works.