How to download the linux kernel 3.14 for imx6sl ???

cancel
Showing results for 
Search instead for 
Did you mean: 

How to download the linux kernel 3.14 for imx6sl ???

200 Views
mutyalaraoneela
Contributor III

Hi All,

Please guide me how to download the kernel 3.14 for imx sololite.

When I am following the document yocto build pdf it is checking out the 3.10 kernel ,

Please help me how to proceed.

Labels (4)
0 Kudos
2 Replies

68 Views
mutyalaraoneela
Contributor III

Thankyou james,

I got the source code and compiled it using

bibtake core-image-base: Images has been created and I copied the .sdcard file to memory card and able to boot from it.

Now I want to cross compile my driver and run on the platform.

For that I have downloaded the toolchain by using the command bitbake meta-toolchain when I am cross compiling the driver with that toolchain I am getting so many error.That I have posted in a new thread

https://community.freescale.com/message/556616#556616


Please suggest me what to do ?? thanks in advance.

0 Kudos

68 Views
jamesbone
NXP TechSupport
NXP TechSupport

All Freescale BSP are located in  GIT server, this is the address

FSL Community BSP

The procedure that you find in the  Yocto Documentation it is the same for the any Kernel the only thing that changes it is the repo of the particular  Kernel version that you are using


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos