HI:
I am doing the dual port lvds display! The lvds0 and lvds1 all connected the one lvds panel.It is also dual channel lvds connection to driver one panel
My boot parameter is as follows:console=ttymxc0,115200 video=mxcfb0:dev=ldb,LDB-T13,if=RGB24,bpp=16 ldb=dul0 ip=dhcp root=/dev/mmcblk0p1 rootwait
I have tried the ldb=spl0 parameters,But the panel cann't display anything.
I used the ldb=dul1 parameters and it can display the image.But it can only display a half picture.
The normal picture is as follows:
So, i have two problem to ask!
First ,how to set the boot parameters
Second ,how to solve the problem about displaying the half image.
你好,楼主,你的问题解决了吗?我现在也遇到类似的问题, 使用的是HDMI显示接口,图片在显示的时候只将图像的下半部分显示到全部屏幕上, 我用的是imx6q芯片,bsp是L3.0.50 应用程序使用时mxc_vpu_test.out
Hi tang yuan
How do you solve your problem? I have the same problem. thank you.
hi,
zhipeng,
I just using the ldb=spl0 parameters ,then it is ok
Hi Tang,
which resolution is your display? Possible modifications of bootargs is change LDB-T13 to LDB-XGA or LDB-1080P60, etc.
Michal
HI:
Michal Susen
My resolution is 1920*720.
LDBi-T13 is accroding my definiton in ldb.c: and board-mx6q_sabresd.c
static struct fb_videomode ldb_modedb[] = {
{
"LDB-T13",60,960,720,20833,
16,16,
8,64,
8,7,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},
}
static struct ipuv3_fb_platform_data sabresd_fb_data[] = {
{
.disp_dev = "ldb",
.interface_pix_fmt = IPU_PIX_FMT_RGB24,
.mode_str = "LDB-T13",
.default_bpp = 16,
.int_clk = false,
.late_init = false,
},
So,i think LDB-T13 it cann't change
Hi Tang,
so change resolution according to your lcd.
static struct fb_videomode ldb_modedb[] = {
{
"LDB-T13",60,1920,720,20833,
16,16,
8,64,
8,7,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},
}
Useful link iMX6QD How to add 24bit LVDS support in Android
Michal
HI:
Michal,I have ever tried the 1920*720,and the result cann't still display normally
Because my lvds is dual port lvds,so i should write 960 not 1920.
Below is my specification:
So ,i should write 960 not 1920
Thanks
HI:
Aravinth,
My BSP is L3.0.35_4.0.0_130424_source.
My kernel version is 3.0.35
Hi tang,
In this "L3.0.35_4.0.0_130424_source" i checked "LDB-T13" this video mode is not there.
And also in your specification resolution they mentioned as 1920x720. So in your bootargs you try to use 720p configuration, it may work.
Regards,
Aravinth
HI
Aravinth,
OK,i try it