I have imx6ul development board with Linux 4.15
I have implemented a splash windows through u-boot, and want to make kernel LCD driver initialization as later as possible.
The current LCD driver is initialized through:
__initcall_mxsfb_driver_init6
Is there a way to call this function through Use Space (Application)? If not, how to implement late initialization?
Thank you,
David Zhou
Hi David
I am afraid it is currently not supported and developing custom codes
may be required, probably as example one can look on implementation of
echo 0 > /sys/class/graphics/fb0/blank on
How do I prevent the LCD from turning off after 20 min ?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------