How to distinguish between Y1 and Y2 devices?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to distinguish between Y1 and Y2 devices?

Jump to solution
1,027 Views
evgenyboger
Contributor II

Hi,

Is there a way to check which i.mx6ULL model the code is executed on: Y1 or Y2? 

More specifically, we need to determine in runtime, either in U-boot or Linux kernel, the presence of 2nd Ethernet controller and 2nd CAN controller. 

The same question goes for i.mx6UL G1/G2 parts.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
916 Views
igorpadykov
NXP Employee
NXP Employee

Hi Evgeny

please create service request:

https://community.freescale.com/docs/DOC-329745

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
917 Views
igorpadykov
NXP Employee
NXP Employee

Hi Evgeny

please create service request:

https://community.freescale.com/docs/DOC-329745

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply