Hello,
Could you please tell me how to display video captured by the OS08A20 camera via HDMI(LT8912)?
GST_DEBUG=3 gst-launch-1.0 v4l2src device=/dev/video0 ! "video/x-raw,width=1920,height=1080,format=YUYV" ! videoconvert ! autovideosink
■ Result
0:00:00.083718541 916 0xaaaaf3247f20 ERROR GST_PIPELINE grammar.y:1138:gst_parse_perform_link: could not link v4l2src0 to videoconvert0, neither element can handle caps video/x-raw, width=(int)1920, height=(int)1080, format=(string)YUYV WARNING: erroneous pipeline: could not link v4l2src0 to videoconvert0, neither element can handle caps video/x-raw, width=(int)1920, height=(int)1080, format=(string)YUYV
If any additional information is needed, please let me know.
Thank you in advance!
I have tried on the i.MX 95 EVK running 6.12.20_2.0.0 BSP, it can run well.
Run the example Gstreamer pipeline to verify camera stream
root@imx95evk:~# gst-launch-1.0 libcamerasrc ! queue ! autovideosink
@Rita_Wang
Thank you for checking.
I tried the GStreamer pipeline you suggested, but I encountered an error.
I will investigate the details of the error.
root@imx95evk:~# gst-launch-1.0 libcamerasrc ! queue ! autovideosink
Setting pipeline to PAUSED ...
[0:01:47.980555800] [624] INFO Camera camera_manager.cpp:315 libcamera v0.0.0+4594-lf-6.6.23-2.0.0-dirty (2025-09-05T01:32:47+00:00)
[0:01:48.031624883] [629] INFO NxpNeo neo_utils.cpp:629 Parsing pipeline config file /usr/share/libcamera/pipeline/nxp/neo/config.yaml
[0:01:48.033805175] [629] WARN CameraSensor camera_sensor.cpp:248 'os08a20 2-0036': Recommended V4L2 control 0x009a0922 not supported
[0:01:48.033880508] [629] WARN CameraSensor camera_sensor.cpp:315 'os08a20 2-0036': The sensor kernel driver needs to be fixed
[0:01:48.033911467] [629] WARN CameraSensor camera_sensor.cpp:317 'os08a20 2-0036': See Documentation/sensor_driver_requirements.rst in the libcamera sources for more information
[0:01:48.034876550] [629] WARN CameraSensorProperties camera_sensor_properties.cpp:262 No static properties available for 'os08a20'
[0:01:48.034923050] [629] WARN CameraSensorProperties camera_sensor_properties.cpp:264 Please consider updating the camera sensor properties database
[0:01:48.034952592] [629] WARN CameraSensor camera_sensor.cpp:461 'os08a20 2-0036': Failed to retrieve the camera location
[0:01:48.034980800] [629] WARN CameraSensor camera_sensor.cpp:483 'os08a20 2-0036': Rotation control not available, default to 0 degrees
Pipeline is live and does not need PREROLL ...
ERROR: from element /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0: Internal data stream error.
Pipeline is PREROLLED ...
Additional debug info:
/usr/src/debug/libcamera/0.2.0.imx/src/gstreamer/gstlibcamerasrc.cpp(645): gst_libcamera_src_task_enter (): /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0:
streaming stopped, reason not-negotiated (-4)
Setting pipeline to PLAYING ...
ERROR: pipeline doesn't want to preroll.
I would appreciate it if you could advise me on anything else I should try or check.
Hi @kazuhito_morita ,
Can you share the board picture to me? I do not know the verison Board in your side, B0 or A1 version, thanks.
Wish you have a nice day
Best Regards
Rita
Hi, @Rita_Wang
Thank you for your cheking.
I’m attaching a photo of the board.
Please take a look and let me know what you think.
best regards.
Hi @kazuhito_morita ,
I see the board you are using, it is not our EVK board, here I will test the OS08A20 camera via HDMI on our EVK board and then tell you the result.
By the way, in China we will have the China National days leave from today and I will test i for you when I back to office on the Oct 9th. Thanks for kindly understandings.
Wish you have a nice day
Best Regards
Rita
Thank you very much for your support.
Wishing you a wonderful holiday!
Thank you for your response.
The box is labeled as follows:
iMX95 Verdin EVK V1.1D
PN: 05241103
SN: 36204509
The board itself is labeled as follows:
iMX95 Verdin EVK CB V1.3A
PN:05211300
SN:35873003
best regards
Thank you for your response.
The box is labeled as follows:
iMX95 Verdin EVK V1.1D
PN: 05241103
SN: 36204509
The board itself is labeled as follows:
iMX95 Verdin EVK CB V1.3A
PN:05211300
SN:35873003
best regards
Can you share the board picture to me?
I tried to capture an image using v4l2-ctl, then the kernel crashed.
When I try to start a video capture using the following command, the kernel crashes (Oops) every time.
v4l2-ctl -d /dev/video0 --stream-mmap=1 --stream-count=1
Internal error: Oops: 0000000096000004 [#1] PREEMPT SMP
CPU: 1 PID: 691 Comm: v4l2-ctl Not tainted 6.6.23-lts-next-06236-gb586a521770e #1
Hardware name: NXP i.MX95 19X19 board (DT)
pc : formatter_subdev_enable_streams+0xb0/0x22c
...
Call trace:
formatter_subdev_enable_streams+0xb0/0x22c
v4l2_subdev_enable_streams+0xe4/0x268
mxc_isi_crossbar_enable_streams+0x12c/0x1d0
v4l2_subdev_enable_streams+0xe4/0x268
mxc_isi_pipe_enable+0x204/0x2ac
mxc_isi_vb2_start_streaming+0xa0/0xe4
vb2_start_streaming+0x68/0x15c
vb2_core_streamon+0xf8/0x1bc
vb2_streamon+0x18/0x64
mxc_isi_video_streamon+0x28c/0x314
v4l_streamon+0x24/0x30
__video_do_ioctl+0x32c/0x3f8
The media graph is active with crossbar/csi/formatter/ISI routing.
(See attached details below. media-ctl.txt)
...
For the i.MX95 19x19 EVK boar which version are you using, B0 or others?