Hello all,
We hava a proble about display gradient effect, the picture shows as below:
computer display normal:
imx6ul board display badly(RGB interface) ,the gradient have ripples on TFT LCD:
our imx6ul board eLCDIF hardware was disigned 24 data line for RBG888 , the DTB configure as below:
&iomuxc {
myimx6a7-lcd-pad {
pinctrl_lcd_lcdif_ctrl: lcd_lcdif_ctrl_grp {
fsl,pins = <
MX6UL_PAD_LCD_CLK__LCDIF_CLK 0x79
MX6UL_PAD_LCD_ENABLE__LCDIF_ENABLE 0x79
MX6UL_PAD_LCD_HSYNC__LCDIF_HSYNC 0x79
MX6UL_PAD_LCD_VSYNC__LCDIF_VSYNC 0x79
MX6UL_PAD_LCD_RESET__GPIO3_IO04 0x79
>;
};
pinctrl_lcd_lcdif_data: lcd_lcdif_data_grp {
fsl,pins = <
MX6UL_PAD_LCD_DATA00__LCDIF_DATA00 0x79
MX6UL_PAD_LCD_DATA01__LCDIF_DATA01 0x79
MX6UL_PAD_LCD_DATA02__LCDIF_DATA02 0x79
MX6UL_PAD_LCD_DATA03__LCDIF_DATA03 0x79
MX6UL_PAD_LCD_DATA04__LCDIF_DATA04 0x79
MX6UL_PAD_LCD_DATA05__LCDIF_DATA05 0x79
MX6UL_PAD_LCD_DATA06__LCDIF_DATA06 0x79
MX6UL_PAD_LCD_DATA07__LCDIF_DATA07 0x79
MX6UL_PAD_LCD_DATA08__LCDIF_DATA08 0x79
MX6UL_PAD_LCD_DATA09__LCDIF_DATA09 0x79
MX6UL_PAD_LCD_DATA10__LCDIF_DATA10 0x79
MX6UL_PAD_LCD_DATA11__LCDIF_DATA11 0x79
MX6UL_PAD_LCD_DATA12__LCDIF_DATA12 0x79
MX6UL_PAD_LCD_DATA13__LCDIF_DATA13 0x79
MX6UL_PAD_LCD_DATA14__LCDIF_DATA14 0x79
MX6UL_PAD_LCD_DATA15__LCDIF_DATA15 0x79
MX6UL_PAD_LCD_DATA16__LCDIF_DATA16 0x79
MX6UL_PAD_LCD_DATA17__LCDIF_DATA17 0x79
MX6UL_PAD_LCD_DATA18__LCDIF_DATA18 0x79
MX6UL_PAD_LCD_DATA19__LCDIF_DATA19 0x79
MX6UL_PAD_LCD_DATA20__LCDIF_DATA20 0x79
MX6UL_PAD_LCD_DATA21__LCDIF_DATA21 0x79
MX6UL_PAD_LCD_DATA22__LCDIF_DATA22 0x79
MX6UL_PAD_LCD_DATA23__LCDIF_DATA23 0x79
>;
};
};
};
&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcd_lcdif_ctrl
&pinctrl_lcd_lcdif_data>;
display = <&display0>;
status = "okay";
display0: display {
bits-per-pixel = <32>;
bus-width = <24>;
display-timings {
native-mode = <&timing0>;
timing0: timing0 {
clock-frequency = <51000000>;
hactive = <1024>;
vactive = <600>;
hfront-porch = <250>;
hback-porch = <160>;
hsync-len = <70>;
vback-porch = <25>;
vfront-porch = <12>;
vsync-len = <12>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <1>;
};
};
};
};
The eLCDIF driver path: drivers/video/fbdev/mxsfb.c
what can i do for it? thanks
I've the same problem with my imx7d-based custom board. I think it's not about timings or hardware pins, I've checked all of things for days.. it's an graphics processing issue, an software issue. However I couldn't solve my problem although I tried 3 different kernels. My 24-bit parallel LCD and Ti's tsc2004 touchscreen working fine except for that gradient trouble!
thanks the reply~
LCD displaying pictures is perfect, besides image that has gradients.
using fbset cmd to get informations about LCD configs in Kernel
mode "1024x600-52"
#
geometry 1024 600 1024 600 32
timings 19607 160 250 25 12 70 12
accel false
rgba 8/16,8/8,8/0,0/0
endmode
I have tried to set dpp:16, dpp:24 and 32, gradients displays not good on LCD-TFT.
witch one to decides the display effect of gradients?
any options tell to me, thanks.
Yes, i have calculated timing parameters according to datasheet support by vendor.
this is our lcd reference manual parts of timing setting.
display-timings {
native-mode = <&timing0>;
timing0: timing0 {
clock-frequency = <51000000>;
hactive = <1024>;
vactive = <600>;
hfront-porch = <250>;
hback-porch = <160>;
hsync-len = <70>;
vback-porch = <25>;
vfront-porch = <12>;
vsync-len = <12>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <1>;
};
};
any you needed i will support if i can.
Looking forward to you reply.
thanks.