How to disable build of u-boot in "core-image-minimal" ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to disable build of u-boot in "core-image-minimal" ?

ソリューションへジャンプ
6,893件の閲覧回数
mb1
Contributor III

In the latest Yocto BSP (4.14.98_ga / sumo) I added a custom machine for our i.MX8M mini machine, added some kernel patches, and some U-Boot patches. All this works fine for i.MX8M Mini. Now I am trying to do this for our i.MX6 based CoMs. It fails when building U-Boot. We don't need U-Boot, because for i.MX6 CoMs we have our own U-Boot. Is there a way when building core-image-minimal to configure "dont build u-boot" ?

Thanks in advance

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
6,458件の閲覧回数
mb1
Contributor III

For now I figured out, how to skip it in current Yocto Sumo release.

Use the following command to skip dependencies u-boot and u-boot-imx in building core-image-minimal.

It is important to say, that IMAGE_FSTYPES_remove = has to contain "sdcard". Sdcard image needs u-boot to work.

bitbake -I u-boot -I u-boot-imx  core-image-minimal

You can also set this as a variable:

 

https://www.yoctoproject.org/docs/current/bitbake-user-manual/bitbake-user-manual.html

 

Let me know if there is any better solution.

Regards

Markus

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
6,459件の閲覧回数
mb1
Contributor III

For now I figured out, how to skip it in current Yocto Sumo release.

Use the following command to skip dependencies u-boot and u-boot-imx in building core-image-minimal.

It is important to say, that IMAGE_FSTYPES_remove = has to contain "sdcard". Sdcard image needs u-boot to work.

bitbake -I u-boot -I u-boot-imx  core-image-minimal

You can also set this as a variable:

 

https://www.yoctoproject.org/docs/current/bitbake-user-manual/bitbake-user-manual.html

 

Let me know if there is any better solution.

Regards

Markus

0 件の賞賛
返信
6,458件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Markus Bauer,

Thank you for sharing your findings! I'm sure they will help other community users.

Theoretically you could also use IMAGE_INSTALL_remove += "u-boot-imx" provided that you take into consideration dependencies like removing the sdcard FSTYPE as you pointed out.


Regards,

6,458件の閲覧回数
Niebel-TQ
Contributor IV

Hello,

from my understanding, recipes providing bootloader - may it be uboot-imx our your private U-Boot clone or whateverer - should add in their recipe:

PROVIDES = "virtual/bootloader"

That way, you are able

- to depend on virtual/bootloader in generic recipes

- to add PREFERRED_PROVIDER_virtual/bootloader = "your bootloader recipe" to select the bootloader in your machine.conf file

Besides that, if you do not need a bootable image, you can of course remove from IMAGE_FSTYPES

Regards,

Markus

0 件の賞賛
返信
6,458件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi Markus Bauer,

One can refer the below link to disable building of U-boot.

https://community.nxp.com/thread/318106 

Regards,

Radhika Somaiya.

0 件の賞賛
返信
6,458件の閲覧回数
mb1
Contributor III

Hey radhika.somaiya@volansystech.com

I've already tried the solutions mentioned there. I don't know what to do with the lines of the files mentioned in the post you linked. Also this post is from 2014, maybe things have changed?

Setting `IMAGE_BOOTLOADER = ""` results in an error also.

Regards

Markus

0 件の賞賛
返信