How to disable Temperature Limit in iMX6 CPU Single Core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to disable Temperature Limit in iMX6 CPU Single Core

4,005 Views
kunalbarot
Contributor I

Hi 

we are using iMX6 CPU single Core, at room temperature(25 C) we read die temperature is 57 C , and No application is running this time except Linux OS. and I believe after 85 C CPU fold-back the its clock when temperature hit the set 85 C,Correct me if i am wrong here.

first Why the temperature is high even i am not running any application, second why alarm point is set 85 C (die temp)

its too low, because i hit 57 C at room  temperature, and in real world it I run this to 65 C ambient , the temperature will go more than 85C ( without running any application) and clock will reduce so hence performance, Correct me here too if i am wrong.

And last if I need to increase its core temperature limit 85 C to (MAX -10C) , Let me know how it can be done in Linux.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

3,269 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kunal

please check AN4579 i.MX 6 Series Thermal Management Guidelines

https://www.nxp.com/docs/en/application-note/AN4579.pdf 

and description of thermal driver in Chapter 25 Thermal Driver attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply