How to defined a ripple range and absolute maximum voltage?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to defined a ripple range and absolute maximum voltage?

ソリューションへジャンプ
1,765件の閲覧回数
t-iishii
Contributor II

Hi

I have some question about definition of ripple range.

It is defined 5% Vp-p of supply voltage average value in Hardware Development Guide.

If VDD_ARM_CAP  average value is 1.27V, ripple spec allowed 1.238V( = 1.27x0.975) ~ 1.301V( = 1.27x1.025).

Is it correct?

If so,

Absolute maximum voltages of VDD_ARM_CAP is defined to 1.3V in Datasheet.

Is it OK that average value is 1.27V of VDD_ARM_CAP because average value is less than 1.3V?

Or is it NG because top of ripple voltage is over a 1.3V?

Best regards,

Ishii.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,624件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

1.27V+-0.0635V (allowed 5%) should be within allowed by datasheet range.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,625件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

1.27V+-0.0635V (allowed 5%) should be within allowed by datasheet range.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,624件の閲覧回数
t-iishii
Contributor II

Dear igor

Thank you for your quick reply.

How about Absolute Maximum Ratings.

Is it applies an average value (i.e. 1.27V)?

Or average value + ripple (1.27V + 0.0653)?

Best regards,

Ishii.

0 件の賞賛
返信
1,624件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

average value + ripple

Best regards
igor

0 件の賞賛
返信
1,624件の閲覧回数
t-iishii
Contributor II

Dear igor

Thank you for your quick response.

I understand a spec definition of datasheet.

Best regards,

Ishii.

0 件の賞賛
返信