How to debug u-boot.imx by SD Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to debug u-boot.imx by SD Card

ソリューションへジャンプ
1,765件の閲覧回数
road_wang
Contributor I

             My I.MX6UL system is running on SD Card,when I modify some codes on U-Boot code and generated new u-boot.imx,for cann't find u-boot.imx on the SD Card,how to update u-boot.imx on SD Card for debug.

0 件の賞賛
返信
1 解決策
1,697件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Wang,

If you modify the u-boot you need to download the new one to your board. You can use the mfgtool to download. If you are using the newest BSP you need to use the tool UUU.

Hope this can do help for you

Have a nice day

Best Regards

Rita

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,697件の閲覧回数
road_wang
Contributor I

but there isn't u-boot.imx on sdcard,I can't copy it to sdcard directly. How can update u-boot.imx on sdcard?

0 件の賞賛
返信
1,698件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Wang,

If you modify the u-boot you need to download the new one to your board. You can use the mfgtool to download. If you are using the newest BSP you need to use the tool UUU.

Hope this can do help for you

Have a nice day

Best Regards

Rita

0 件の賞賛
返信
1,697件の閲覧回数
road_wang
Contributor I

Hi Rita,

 Because my board nand flash size is only 256M,but the image build from Yocto project is larger than it,So I only use sdcard to debug now. Can update u-boot on SDCard?

Best Regards

Road

0 件の賞賛
返信
1,697件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, if your board support sdcard, you can use it.

0 件の賞賛
返信