How to debug imx6 ipu.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to debug imx6 ipu.

3,959 次查看
guanliangding
Contributor III

Hi, all:

     Now we status is that. adv7282m->imx6d, MIPI input is 576i, vc = 1。

MIPI-CSI2 reg dump:

0x3130302a

0x0

0x1

0x1

0x1

0x300

0x0

0x0

0x0

0x0

0x0

0x0

0x0

0x2626

CSI2IPU reg dump:

0x4

IPU_CM reg dump:

imx-ipuv3 2400000.ipu: IPU_CONF =0xA0000006
imx-ipuv3 2400000.ipu: IPU_INT_CTRL_1 =0x80100000
imx-ipuv3 2400000.ipu: IPU_INT_STAT_1 =0x00000000

IPU_CSI reg dump:

imx-ipuv3 2400000.ipu: CSI1_SENS_CONF =0x02000A02
imx-ipuv3 2400000.ipu: CSI1_SENS_FRM_SIZE =0x027002CF
imx-ipuv3 2400000.ipu: CSI1_ACT_FRM_SIZE =0x027002CF
imx-ipuv3 2400000.ipu: CSI1_MIPI_DI =0xFFFFFF5E

IPU_IC reg dump:

imx-ipuv3 2400000.ipu: 0x00000001

imx-ipuv3 2400000.ipu: 0x22BA2000

imx-ipuv3 2400000.ipu: 0x20002000

imx-ipuv3 2400000.ipu: 0x20002000

imx-ipuv3 2400000.ipu: 0x00000000

imx-ipuv3 2400000.ipu: 0x00000000

imx-ipuv3 2400000.ipu: 0x00000001

imx-ipuv3 2400000.ipu: 0x0000023F

imx-ipuv3 2400000.ipu: 0x000002CF

imx-ipuv3 2400000.ipu: 0x00000000

     But, it is doesn't work anyway.

标签 (1)
0 项奖励
回复
4 回复数

2,618 次查看
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

IPU debug steps are described on p.115 presentation

https://community.freescale.com/docs/DOC-100482

As for adv7280:

1. the adv7280 should be enabled after mipi_csi2_reset().

2. For MIPI CSI input, the clock mode in IPU_CSI_SENS_CONF must be gated clock mode.

          p->u.bt656.clock_curr = 1;

3. For interlaced input, IDMAC 0 should be set to interlaced mode:

"params.csi_mem.interlaced = true;" For progressive input, IDMAC 0 shoudl be

set to progressive mode: "params.csi_mem.interlaced = false;"

          case IPU_CSI_CLK_MODE_GATED_CLK:

in file drivers\media\video\mxc\capture\ipu_csi_enc.c, function csi_enc_setup().

4. For device type:

     adv7280_data.sen.pix.priv = 1;  /* 1 is used to indicate TV in */

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,618 次查看
guanliangding
Contributor III

Hi igor:

     I also have problem, why the adi official adv7282m driver is doesn't work in freescale platform. Adi official  declare that it is a standard interface driver.

0 项奖励
回复

2,618 次查看
igorpadykov
NXP Employee
NXP Employee

seems this is high level driver, while it should be also supported by

low level (means from processor side - i.MX6 IPU/MIPI).

0 项奖励
回复

2,618 次查看
guanliangding
Contributor III

Hi igor:

     Thanks!

     I dump the debug information, but not found any information about drivers\media\video\mxc\capture\ipu_csi_enc.c. Is it means?

0 项奖励
回复