How to cross-compile and optimize gstreamer for imx6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to cross-compile and optimize gstreamer for imx6?

3,119 次查看
tejasshah
Contributor III

Hello,

I have a wandboard-dual board and I am using yocto to compile the source code.

I already have gstreamer installed in my image but I need to just optimize.

Since I already have gstreamer in my image, can I use yocto to optimize gstreamer?

I read about optimization and found that there are three levels -o1, -o2 and -o3 and there

is -os(this optimizes depending on the size and not speed). I just have to optimize the gstreamer

code by adding a flag(which I guess would be putting -o1, -o2 or -o3).

If optimizing gstreamer using yocto is not possible, I will have to cross-compile gstreamer.

Can anyone please tell me, how would I cross-compile gstreamer?

标签 (5)
0 项奖励
回复
2 回复数

1,611 次查看
pchevalier
Contributor I

I'm interested too !

How to cross compile gstreamer 1.2 with freescale plugins for imx6 ?

Where i can download the source of the freescale plugins for gstreamer 1.2 ?

0 项奖励
回复

1,611 次查看
dmitrypozhidaev
Contributor III
0 项奖励
回复